2008-06-27 5:39 AM
2011-05-17 2:52 AM
Ciao,
I've just designed a simple board with a uPSD3233 with only a crystal, pullup resistors on the JTAG port and an RC circuit for the RESET. All the other pins are connected to wirewrap connectors. The idea is to use this simple board for some trainings. Unfortunately, I cannot communicate with the device. With FLINK I always get ''Unable to connect with JTAG target device'' error. Am I missing something simple but really important? Could it be the RESET circuit too simple? Thanks