Posted on May 17, 2011 at 12:07Ciao, I have problems in using the RLINK to program a uPSD3233B on board. I'm able to erase , execute a blank test, and on a programmed part execute the verify, but when I try to program it I always get the following e...
Posted on May 17, 2011 at 12:06I've used bin2hex tool, to convert a binary file I got from my customer into the hex format. With this, I've generated my obj file and programmed my board with FlashLink. The programming was good, but the board is not ...
Posted on May 17, 2011 at 12:05I just started to play with PSDsoft, and I need help in order to generate an SVF or JSTAPLE file. I need to program an uPSD3233 using an ICT test platform via the JTAG interface. The PSDsoft provides this output, but I...
Posted on May 17, 2011 at 11:52Ciao, I'm having an increasing number of devices (uPSD3233B), which are not working properly after they've been programmed. In particular, if I try to verify one of these devices using the FL101, I get in 80% of the ti...
Posted on May 17, 2011 at 11:52Ciao, I've just designed a simple board with a uPSD3233 with only a crystal, pullup resistors on the JTAG port and an RC circuit for the RESET. All the other pins are connected to wirewrap connectors. The idea is to us...