2006-07-10 5:02 AM
2006-06-19 6:05 AM
I have just downloaded the last release 3.3.2 of STVD7.
A workspace saved with STVD7 3.1.1 is no more compilable (I have Cosmic 16K-limited free compiler). It seems that the compiler is launched with a wrong command string: the path of the compiler include folder does not have the '-i' prefix, so the compiler takes the path as a wrong file name and exits with an error. Instead, the tutorial examples are compiled well, the compiler include folder path has the '-i' prefix, so I think is an import matter of the project file .stp. Do you know the right procedure to import 3.1.1 workspaces in STVD7 3.3.2?2006-06-20 2:42 AM
If i get problems with upgrading to a newer version of Visual Develop i find pressing the defaults button on the various project settings tabs fixes the problem.
Regards sjo2006-07-10 5:02 AM
Hi,
When we meet such problems during integration phase, we often see that opening the project settings, navigating in each tab, and clicking on OK is enough to fix the issue. Anyway, this should not happen. Could you send me the *.stp.bak file (backup of the initial stp file). So we could investigate. Emmanuel.