2006-03-27 11:30 PM
main VR OFF issue and power consumption of STDBY at V18bkp
2004-11-10 1:43 PM
I have two more questions about power management.
1. as stated on page 75 of user manual v4, “the PLL is automatically disabled when….� So, if we use our own external 1.8v source and turn off the Main VR, that will cause PLL off and limit the max. operating frequency to 1 MHz ? It doesn’t make sense to turn off the PLL if we use external 1.8v source.. 2. If we use V18bkp for Standby mode voltage source with RTC on, what's the power consumption measured at V18bkp under Standby mode ? The power consumption listed in datasheet seems to be measured at V33 that is not what we want. thanks for your help !2004-11-14 5:41 PM
2005-05-16 8:48 PM
Hello everybody
I have the same question: what's the power consumption of standby at V18BKP?2006-03-27 11:30 PM
Hello everybody
I have the same question: what's the power consumption of standby at V18BKP? Can i use 3.3V battary to supply 1.8V for V18BKP pin and 3.3V for V33 pin when str71x is in STANDBY mode?