2008-01-29 7:34 PM
2011-05-17 12:49 AM
Is it possible to DMA from the MAC directly to memory attached
via EMI? I can't find anywhere in the documentation that explicitly states if this is possible or not. I know that the general purpose DMA can do it but what about the DMA assigned to the ethernet MAC? Thanks in Advance, Victor2011-05-17 12:49 AM
Nobody knows?? Bummer. The 96k of SRAM is not a huge
amount of memory and maintaining TCP connections with 3 concurrent hosts will mean we need way more than the STR9 has which is why we are hanging memory off of the EMI for network buffering. So far the only way I can see to implement this is to have TX/RX buffers in SRAM and then move the data to external mem. It would be great though if the MAC could transfer it to external memory without processor intervention. Any ideas? Victor Valencia Element Labs2011-05-17 12:49 AM
That is essentially what we do (but in reverse):
* external device writes to asynchronous FIFO part * STR912 DMA via EMI to SRAM (in 1k chunks) * then use ENET library ENET_TxPkt( void * ppkt, u16 size )which I've modified to have multiple ENET descriptors (note: search for other threads regarding this) void ENET_TxDscrInit(void) { u32 currIndex; // index to the current descriptor u32 nextIndex = 0; // index to the start of the next descriptor in the // chain u8 * pNextBuffer; // pointer to the RX next buffer in memeory ENET_DMADSCRBase * pCurrentDescr; ENET_DMADSCRBase * pNextDescr; for ( currIndex = 0; currIndex < NUM_TX_BUFFERS; ++currIndex ) { if ( (++nextIndex) == NUM_TX_BUFFERS ) // for the last descriptor nextIndex = 0; // loop back to the first buffer. pCurrentDescr = &dmaTxDscrBase[ currIndex ]; pNextDescr = &dmaTxDscrBase[ nextIndex ]; pNextBuffer = (u8*)(TxBuff + (currIndex * EMAC_MAX_PACKET_SIZE)); /* Initialize ENET status and control */ pCurrentDescr->dmaStatCntl = 0; /* ENET Start Address */ pCurrentDescr->dmaAddr = (u32)pNextBuffer; /* Next Descriptor Address */ pCurrentDescr->dmaNext = (u32)pNextDescr | DMA_DSCR_NXT_NPOL_EN; /* Setting the VALID bit */ pCurrentDescr->dmaPackStatus = 0;//DMA_DSCR_TX_STATUS_VALID_MSK; } TxDscrIndex = 0; /* Tx next set to Tx decriptor base */ ENET_DMA->TXNDAR = (u32)&(dmaTxDscrBase); /* Enable next enable */ ENET_DMA->TXNDAR |= DMA_DSCR_NXT_NPOL_EN; }2011-05-17 12:49 AM
Thanks for the response. I think that our situation is
not quite the same in that you are using the general purpose DMA engine to transfer from EMI. I want to transfer from SRAM to EMI using the MAC-DMA channel. Maybe it will work anyway. I don't know. Victor2011-05-17 12:49 AM
Unless i am mistaken on what you are trying todo - internal SRAM to external memory is just a memory to memory transfer.
The fact that you are using emi does not matter - it is a memory mapped device. Cheers Spen