cancel
Showing results for 
Search instead for 
Did you mean: 

M95M04-A145

suuulx
Associate

Does the M95M04-A145 chip support data erasure at 145℃?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @suuulx, to the community!

Yes, you can erase the M95M04-A145 at max 145°C. However, please bear in mind that this is the maximum temperature and affects the write cycle endurance, which is then only 100k cycles (see data sheet, table 8).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @suuulx, to the community!

Yes, you can erase the M95M04-A145 at max 145°C. However, please bear in mind that this is the maximum temperature and affects the write cycle endurance, which is then only 100k cycles (see data sheet, table 8).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks!