2005-01-19 8:50 PM
2005-01-19 12:19 AM
Hi all
Can any body help me out with SPI code as i am new to this . Looking forward for the code, Thanks in advance2005-01-19 11:27 AM
Are you talking about software or hardware spi ?
Have a look at the following appnotes in the download section AN 970, AN 972 and also the st7 library Regards sjo2005-01-19 7:56 PM
Hi
i am talking about the software SPI which will help in communicating MCU with the External components on the board. thanks2005-01-19 8:50 PM
AN972 gives details of a software spi master, a slave device is a lot more complicated and would be better done using the hardware spi cell. Can you not use this as it is present on all st7's
Regards sjo