2006-07-31 11:04 PM
2011-05-17 12:30 AM
Hi,
I'd like to try to erase my flash using jtag. But so far I did not find any infos about the jtag commands. Anyone got a link ? Edited: Found it on the st912 page. Now trying if I can get on the flash using j-link.[ This message was edited by: 42Bastian on 28-07-2006 17:26 ]2011-05-17 12:30 AM
Hi,
There is a seperate STR9 flash programming manual available from this website. Martin.2011-05-17 12:30 AM
�es, found it.
Now , as I wrote, I have to figure out how to attack it. My only device I have is a J-Link with some SW. But so far I don't seem to have the correct codes sent. I even do not get the IDCODE. My computer has no parallel port anymore, so the ST JTAG solution does not work. I am close to using another ARM board :)2011-05-17 12:30 AM
What software are you using with the JLINK, is it not IAR ? Perhaps you are using the free gdb server available on the net.
The jtag config of the str9 is as follows: 3 taps are present, scan chain (ir 5 bits), arm966 core (ir 4 bits) and flash controller (ir 8 bits). I have added support to Openocd for the str9 and this should be available in svn very soon. Also the str9 (arm966) is a strange beast, the monitor mode is enabled at reset ? unlike other arm9 cores. This has to be disabled before breakpoints etc can be enabled. Regards sjo2011-05-17 12:30 AM
I downloaded a SW collection from segger.
Anyway I will look at openOCD. I meanwhile als tried iSystem, but so far I have no luck in getting anything meaningfull back from either my str9 nor from a LPC2294. I am really close to writing my own tool.