2004-12-12 7:10 PM
2004-12-07 6:55 PM
Hi all,
is there any software to program the internal and the external flash of the STR710 without using the RealView Developer Kit? I need a software for end-of-line programming, so the RVDK is not the right software, as I need a batch or script configurable tool for flashing. Maybe there actually is some flash software that works with a wiggler-compatible interface? thanks for your help, Marcus2004-12-07 10:04 PM
Hello,
for programming tool, there's two offers from 3rd parties: 1.Memtool from PLS (www.pls-mc.com) standalone software interface that can be integrated in automatic environment. y 2. J-flasher from Segger (www.segger.com) (standalone software interface used with j-link ) Regards2004-12-12 7:10 PM
That sounds good,
thank you