2002-10-22 7:49 AM
ICP programming of the E2 memory of a ROM device (ST6265)
2002-10-22 7:33 AM
I am planing to go in production with the ST6265 ROM.
Can I read and program its E2 memory (calibration) using ICP ? The documentations I found on internet only allow it for Eprom and OTP devices. Breizh2002-10-22 7:49 AM
Yes, it works. I have made my tests based on the ICP application note (see AN593) which only refers to Eprom and OTP devices.
For your information, I was able to read and program the EEPROM even though the read-out protection was activated. Take care