2003-10-14 9:18 PM
HW problem with ST623 Starter Kit
2003-10-12 11:45 PM
Hi all,
after putting the power jack into the board, a blaze occurred and I'm not able to run the demos. (only the power LED is on). I tested the power in the board and it seems ok. I cheked the communication between the MCU adn the PC with WinEpromer, and I'm able to read the program inside the demo MCU. Any Idea? Thank's Claudio2003-10-14 6:56 PM
For the demo to work properly, read ''Running the demonstration Programs'' in ST623X kit manual(page 19,20,21).
Check that: 1.ST6232 Programmed with demo32.hex must be plugged into the socket. 2.The kit should be in the user mode. Let me know if you still faced the problem.2003-10-14 9:18 PM
Before the blaze I ran the demo without any problem, is it possible that something has been broken in the MCU?
Addictional question: How can I do in order to use LED indicators, UART port and 7-segment display with the socket of 6230? I verified that there is no link between yhe socket and the jumpers or the I/Os pin in the board