2003-09-26 3:04 PM
how to use ST7262 timer interrupt.....
2003-09-23 7:33 PM
Hi! I have some problem in ST7262 programming...
I want to use timer interrupt every 1sec. What register should I enable and how do I use timer function? If anyone know this in C language, plz tell me!. I will very appreciate your help!!2003-09-26 3:04 PM
if you use the Hiware, you can do it
/*----------------------------------------------------------------------------- ROUTINE NAME : INT_TIM DESCRIPTION : Comes from the TIM cell. -----------------------------------------------------------------------------*/ #pragma TRAP_PROC // SAVE_REGS void INT_TIM(void) { if (TSR & 0x40) { asm LD A,OCLR1 asm LD CRL, A // Reset the free counter Clock_Tick++; PDDR ^= 0x20; } else if (TSR & 0x20) { asm LD A, CRL; // Clear TOF anyway asm LD A, OCHR2 asm LD A, OCLR2; // Clear OCF2 anyway } }