cancel
Showing results for 
Search instead for 
Did you mean: 

How to set the gain of the TDA7491 HV 30/31 pin GAIN 0/ GAIN pin?

ouyang
Associate

How to set the gain of GAIN0/GAIN1 pins 30/31 of TDA7491HV?

ouyang_0-1741596400626.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @ouyang, to the community!

You can configure the two pins according to the desired closed-loop gain. According to the data sheet, table 7, you can choose between 20/26/30/32dB.

In the picture you have inserted, both pins are set to VDDS = H, which corresponds to an open-loop gain of 32dB.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @ouyang, to the community!

You can configure the two pins according to the desired closed-loop gain. According to the data sheet, table 7, you can choose between 20/26/30/32dB.

In the picture you have inserted, both pins are set to VDDS = H, which corresponds to an open-loop gain of 32dB.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AScha.3
Chief III

See ds , figure 22 :

Gain settings: 0+0 V -> 20dB , 3+3 V -> 32dB , etc.

If you feel a post has answered your question, please click "Accept as Solution".