2025-03-10 1:49 AM - last edited on 2025-03-10 1:58 AM by mƎALLEm
2025-03-10 2:46 AM
Welcome @ouyang, to the community!
You can configure the two pins according to the desired closed-loop gain. According to the data sheet, table 7, you can choose between 20/26/30/32dB.
In the picture you have inserted, both pins are set to VDDS = H, which corresponds to an open-loop gain of 32dB.
Does it answer your question?
Regards
/Peter
2025-03-10 2:46 AM
See ds , figure 22 :
Gain settings: 0+0 V -> 20dB , 3+3 V -> 32dB , etc.