2024-11-28 1:10 AM - edited 2024-11-28 1:17 AM
Hi, I'm currently working on a project using the "Black" STM32F407VET6 board, and on the lookout for a good 7" touchscreen display and 5 MP camera choice.
For the display, I'm considering an 800x480 SSD1963 based touchscreen panel that can connect to the LCD connectors on the board.
What exactly should I look for? Reading older posts, I'm aware that the STM32F407VET6 not having a lot of onboard memory is a concern, and displaying a UI with LVGL isn't the only thing I want to do. I plan to use Zephyr OS and there will be some PWM controller code that will have to live alongside the display stuff.
For the camera, I came across this post that links to AN5020 and recommends a 5MP OV5642 based camera. My requirement is also 5MP so I think that would work for me.
Would appreciate any help regarding points I should be considering, reducing memory usage and if this kind of system sounds feasible on this particular platform.
Thanks
2024-11-28 2:05 AM
@ose7b wrote:the "Black" STM32F407VET6 board,
anyone can make a black board!
Is it one of these:
please give a link to the one you're actually using.
2024-11-28 2:07 AM
this is the Zephyr device page for my board: https://docs.zephyrproject.org/latest/boards/others/black_f407ve/doc/index.html
2024-11-28 2:27 AM
More useful to have the supplier page for the board you actually have.
Does the board documentation not give a specification for the supported LCDs (vain hope) ?
2024-11-28 2:41 AM
I have ordered the board from this supplier: https://robu.in/product/stm32f407vet6-arm-cortex-m4-core-with-dsp-and-fpu/
The datasheet they link to is just the microcontroller datasheet. In there I just see that it has a FSMC interface with 8080/6800 modes.
Also found this page https://stm32-base.org/boards/STM32F407VET6-STM32-F4VE-V2.0.html but doesn't seem very useful.