2006-09-16 4:50 PM
Help: HDLC with FM0/MANCH encoding
2006-09-16 4:50 PM
Hi All,
My code work well with NRZ/NRZI encoding, but can't work with FM0/MANCH encoding. Can anyone help me? thank you very much! here is the code : //============================================================================= #define CODE_NRZ 0 #define CODE_NRZI 1 #define CODE_FM0 2 #define CODE_MANCH 3 void HDLC_Init(unsigned char tx_code,unsigned int tx_bps,unsigned char rx_code,unsigned int rx_bps) { HDLC->GA1 = 0; HDLC->GA0 = 0; HDLC->GAM1 = 0; HDLC->GAM0 = 0; HDLC->PRES = 0; HDLC->POSS = 0; HDLC->TCTL = 0; HDLC->RCTL = 0; HDLC->BRR = 0; HDLC->PRSR = 0; HDLC->TFBCR = 0; HDLC->RFBCR = 0; HDLC->PCR = 0; HDLC->ISR = 0; HDLC->IMR = 0; HDLC->PARH = 0; HDLC->PAMH = 0; HDLC->PARL = 0x00AA; HDLC->PAML = 0x00FF; GPIO_Config (GPIO1, 0x2000, GPIO_IN_TRI_CMOS); GPIO_Config (GPIO1, 0x4000, GPIO_IN_TRI_CMOS); GPIO_Config (GPIO1, 0x8000, GPIO_AF_PP); if((tx_code==CODE_NRZ)||(tx_code==CODE_NRZI)) { HDLC->TCTL = (((unsigned short)1)< HDLC->BRR = ((RCCU_FrequencyValue(RCCU_FCLK)/tx_bps-1) & 0x0FFF); } else //((tx_code==CODE_FM0)||(tx_code==CODE_MANCH) { HDLC->TCTL = (((unsigned short)1)< HDLC->BRR = ((RCCU_FrequencyValue(RCCU_FCLK)/tx_bps/2-1) & 0x0FFF); } if((rx_code==CODE_NRZ)||(rx_code==CODE_NRZI)) { HDLC->RCTL = (((unsigned short)1)< HDLC->PRSR = ((RCCU_FrequencyValue(RCCU_FCLK)/rx_bps-1) & 0x00FF); } else //((tx_code==CODE_FM0)||(tx_code==CODE_MANCH)) { HDLC->RCTL = (((unsigned short)1)< HDLC->PRSR = ((RCCU_FrequencyValue(RCCU_FCLK)/rx_bps/2-1) & 0x00FF); } }