2022-08-08 5:21 AM
2022-08-11 7:30 AM
Oh, it looks like there's a typo in the data sheet: page 1, Product Summary, mentioned in the last two lines:
should be read as:
But table 7, ordering information correctly lists the options of the pin-out.
Yes, you can use your diagram with the red marked pin numbers for this part number.
Regards
/Peter
P.S.: It is permissible, but it is still not a good idea to reply by email to messages from the community, because the reply email usually sends all private data (telephone numbers, addresses, etc). This is then visible to everyone in this community, which is open to the public worldwide. To ensure data protection, you should therefore not reply by email, but via the community's web interface.
2022-08-08 2:20 PM
Welcome, @PKala.3, to the community!
On pages 1 and 9 of the data sheet you will find the note "base and emitter are inverted for 2N5154RSRHRx and 2N5154SRHRx series".
The word inverted is a bit unfortunate, because it actually refers to a logical function, but here it means the exchanged function of base and emitter.
Does it answer your question?
Regards
/Peter
2022-08-09 12:18 AM
Dear Mr. Bensch,
Thank you for your reply.
Could you please confirm that on the P/N: 2N5154RSRHRG, the emitter is on pin2 and not on pin1 (as it is mentioned on the table of Product Summary (column ‘Remarks’))?
Can we use the following diagram for this part number?
Freundliche Grüsse / Kind regards
Panagiotis Kalaitzidis
2022-08-11 7:14 AM
Dear Mr. Bensch, could you please confirm the above?
Best regards,
Panagiotis Kalaitzidis
2022-08-11 7:30 AM
Oh, it looks like there's a typo in the data sheet: page 1, Product Summary, mentioned in the last two lines:
should be read as:
But table 7, ordering information correctly lists the options of the pin-out.
Yes, you can use your diagram with the red marked pin numbers for this part number.
Regards
/Peter
P.S.: It is permissible, but it is still not a good idea to reply by email to messages from the community, because the reply email usually sends all private data (telephone numbers, addresses, etc). This is then visible to everyone in this community, which is open to the public worldwide. To ensure data protection, you should therefore not reply by email, but via the community's web interface.