2024-05-29 8:58 AM
Hello,
I have recently purchased an BMW F650GS motorcycle. Now there has been a rather amateurish fix to the fuel pump.
Where it is now connected parralel over the rear light.
The ECU feeds the pump via an VN31 30F922 (transistor?)
Im trying to diagnose of the component has failed and can be replaced (with an alternative) or that the fault is from a different source in the ecu. However i can't seem to find a datasheet.
Is there any way to find a datasheet so i can know what to expect on the 5 pins?
Gr Evert
Solved! Go to Solution.
2024-05-29 9:40 AM
The second line is production/plant and date codes, refer to the standard data sheet.
2024-05-29 9:40 AM
The second line is production/plant and date codes, refer to the standard data sheet.
2024-05-29 10:18 AM - edited 2024-05-29 10:37 AM
Thank you so much! I tried to search for it and then got airplanes.
As for the component if anyone is interested. the the voltages were normal but the input isnt activated. So the fault lies elsewhere.
Thanks again!