2024-10-09 5:12 PM
Hello, I have looked many places, including Google and the ST website, and I cannot find this microcontroller anywhere. Markings on this controller are the following:
6242MCH
HES-02-03
M22050431A
if someone can provide any information on this and a datasheet, that would be very useful!
2024-10-09 5:31 PM
Probably searching on the wrong data, perhaps provide a picture, large, clear and in focus. Show usage context, package and pin count details.
If automotive application might be a custom or proprietary chip.
2024-10-09 5:52 PM
attached 64 pins. It’s not automotive application. It is an older stereo application. This is all the information I have.
2024-10-10 10:50 AM
As @Tesla DeLorean has already surmised, this is a customised device to whose documents and data only the customer placing the order has or had access.
I'm sorry I can't give you a more pleasant answer.
Regards
/Peter
2024-10-10 1:23 PM
I think I can help you
2024-10-10 1:29 PM
Any help is appreciated. Thanks