2007-09-25 2:16 PM
2007-09-25 2:16 PM
Hi,
I am using 72F264G2 with an 8MHz crystal. I have the following code: int main(void) { DisableInterrupts; SetBit(PADDR,7); // Test output bit SetBit(MISCR1,4); // set input sensitivity SetBit(MISCR1,3); ClearBit(PCDDR,3); SetBit(PCOR,3); // set pull-up input to generate interrupt EnableInterrupts; while (1) { Halt; } } @interrupt void Ei0Interrupt(void) { PA7=PC3; return; } The CPU is fed a square signal on PC3 from a function generator. The Interrupt routine then copies the input signal to another pin (PA7) and both signal are observed on the oscilloscope. I observe a delay of about 1 milisecond. I guess this is what it takes the CPU to go from HALT to RUN, but it seems to me a bit long. Am I correct? I read somewhere on the forum that it takes 256 cycles to go from HALT to RUN mode Thanks