2004-09-16 2:44 AM
2004-09-15 6:04 PM
dear sjo,
I have maked one FLASHBASH(use St72C264G2), but it doesn't work. it failed when I use ''FLASHBASH windows software''. I have used the the new version of pcb and and withot serial communication my pcb works. it seems that falshbash software on windows can not communicate with the pcb. when i try to do every funtion wich needs to communicate with pcb I get the failed message. would you please help me to solve this problem. regrds S.E.Alavi2004-09-16 2:44 AM
Both the hardware and software have been extensivly tested so double check your pcb and software versions.
If you have built the source then check #define SOFTUART has been commented out if using the 264. The s19 files on the website are built by default for the 264 (from v1.07). Regards sjo