2008-07-18 1:14 AM
error in the STR9 library?..............91x_emi.c
2011-05-17 12:54 AM
By carefully debugging our emi and enet initialisation we found that the void EMI_StructInit( EMI_InitTypeDef *EMI_InitStruct) function in 91x_emi.c does not initialise the EMI_BurstModeWrite_TransferLength element.
Even though the EMI_BurstModeWrite_Selection is set to EMI_NonBurstModeWrite we think EMI_BurstModeWrite_TransferLength must also be set to EMI_Write_4Data. The code ''EMI_InitStruct->EMI_BurstModeWrite_TransferLength = EMI_Write_4Data''; should be added to the EMI_StructInit() function. In general _ALL_ the elements of a structure should be initialised in the StructInit() functions otherwise very strange results will occur. As the various StructInit() calls are processed at the beginning of the code the structure elements are pushed into the stack area. Any element not implicitly set will pick up a random value left there by a previous call. So you can track the file version we are using here is the header from the library file: /******************** (C) COPYRIGHT 2007 STMicroelectronics ******************** * File Name : 91x_emi.c * Author : MCD Application Team * Version : V2.0 * Date : 12/07/2007 * Description : This file provides all the EMI firmware functions. ******************************************************************************** and /******************** (C) COPYRIGHT 2007 STMicroelectronics ******************** * File Name : 91x_emi.h * Author : MCD Application Team * Version : V2.0 * Date : 12/07/2007 * Description : This file contains all the functions prototypes for the * EMI firmware library. ********************************************************************************2011-05-17 12:54 AM
Hi
you are right :D recently I found a very strange behavior of EMI, when EMI_InitTypeDef EMI_InitStruct; was local external memory didn't work but when it was global it worked fine :-? I read your post and I know now when its local content of the EMI_InitStruct->EMI_BurstModeWrite_TransferLength field is unpredictable and when EMI_Init writes EMI_Bankx->BCR &= EMI_BurstModeWrite_TL_Mask; EMI_Bankx->BCR |= EMI_InitStruct->EMI_BurstModeWrite_TransferLength; it corrupts all fields in BCR register but when its global its zeroed and everything looks good Thanks Norbert