2008-03-05 5:56 PM
2008-03-05 2:38 AM
Is there an errata sheet for the STR712, or are there no known silicon issues ?
[ This message was edited by: bruno.berger on 05-03-2008 16:09 ]2008-03-05 5:56 PM
I can't give an answer to the question, but I can share my personal experience with the STR710FZ2 MCU. First, ST removed all mentions of the HDLC feature from datasheet and manual, which did not work properly, apparently. Second, when I attempted to use the flash end-of-write interrupt, I discovered that it didn't work properly, and ST's reaction to that was an announcement in the forum saying 'don't use the feature.' So, the absence of errata does not necessarily mean no issues in silicon. From my experience, you'd have to hunt for the information, which is a sad state of affairs.