cancel
Showing results for 
Search instead for 
Did you mean: 

ECMF02-4CMX8 - pin connection for USB type C application

Hi,

I want to use ECMF02-4CMX8 as ESD protection and filtering means for a isolated USB 2.0 downstream port design.
The chosen connector is a Type C receptacle.
My question pertains to pin function of ECMF02-4CMX8.
The type C connector exposes two configuration pins, CC1 and CC2.
Can I connect CC1 to pin 4 and CC2 to pin 1 ?
From the datasheet I know the pin 1 is reserved to VBUS and pin 4 is reserved to ID, however I prefer to assign this 1 pin to CC2, and route VBUS to a separate over-voltage protection chip (MAX14699EWC+).
Is my choice correct and safe ?
I attach the proposed schematic for the complete interface.

Thank you for any help
Gabriele

1 REPLY 1
MROUV.1
ST Employee

Hi Gabriele,

 

Good idea !

CC1 and CC2 can be protected with ID and VBUS pin of ECMF02-4CMX8.

 

Embedded ESD protection for ID and VBUS are not identical.

VBUS is more capacitive (19pF) and much more robust 2.5A 8/20µs.

In any case, both protections do not impact normal behavior of Type-C.

 

It is key to protect CC1 and CC2 if these lines are used to sense the adapter current capability (0.5A or 1.5A or 3.0A) according to the CC1 or CC2 line voltage.

MROUV1_0-1737640929615.png

If not used, then ECMF2-40A100N6 (QFN-6L) can be used. R20 and R21 do not require ESD protection.

 

Last comment, to protect the MAX14699 against surges, I recommend to place ESDA25P35-1U1M between VBUS and GND.

 

Best regards,
Mathieu