2004-10-07 09:46 PM
DVP3 Emulator: problem with shared supply tension!Help
2004-10-06 03:53 AM
I must to simulation ST7LITE19M with ST7-DVP3.
In PA7 and PB6 there are 2 buttons,open and close, that pull-up the voltage at 5V. In interrupt will be capture they. Problem:when i push open (pull-up 5V) the button close pull-up a 1,6-2 volts???? Result:both buttons are pushed!!Don't run! Is it a problem of shared power supply tension? Solution? Thanks a lot!2004-10-07 03:18 AM
Can you pls re-frame yr question ? I havnt used the DVP but..
When you say '' when i push open (pull-up 5V) the button close pull-up a 1,6-2 volts???? Result:both buttons are pushed!!'' What exactly you mean ? isnt it a mechanical problem.2004-10-07 09:46 PM
No mechanic problem but electric problem.
2 input floating. When i connect 1 input at 5v other input pull-up at 1 volt. I have resolving: Emulator dont like over tension on other pin. In other input pin i have 5,6v (Vdd=5). I have diminished the tension on other pin (5,6 -> 4,5) and the emulator is OK.