2006-02-09 1:23 AM
Cosmic compiler, not completely right behaviour?
2006-02-08 10:06 PM
Hello, All.
I discovered a little bit wrong behaviour of Cosmic compiler V4.5c.1 - 20 Jun 2005. Let's examine following functions. They differ no so much. 1) void my_func(unsigned char i) { unsigned char j; j = i; ... } 2) void my_func(unsigned char i) { unsigned char j; _asm(''ld a,0''); j = i; ... } Value of j should be in both cases the same. But in practice it is not true. Why? Let's take a look in asm code. 1) ;void my_func(unsigned char i) ;{ switch .text _my_func: push a OFST: set 257 ;j = i; ld x,s ld (OFST+0,x),a ... ;} 2) ;void my_func(unsigned char i) ;{ switch .text _my_func: push a OFST: set 257 ;_asm(''ld a,0''); ld a,0 ;j = i; ld x,s ld (OFST+0,x),a ... ;} The function parameter i is stored in register a and on stack. In the 1st case as far as register a keeps value of i compiler uses it to fill variable j. But in the 2nd case register a are „corrupted“ by _asm function. Compiler doesn't analyse this code and skips it. That's why variable j gets a wrong value, in this case allways „0“. Ok, we can prevent such sutiation by loading register a with value of parameter i ( _asm(''pop a\n push a'') or something else). I would like to have more nice solution. Is it a bug or a feature? Do any compiler keys or parameters exist to make it analyse inlined asm code? Tnx, Luter2006-02-09 12:09 AM
Luter,
the compiler always assumes that any inline asm does not break any resource; if you do (in your case the A register), it's up to you to save and restore what you break. Regards, Luca2006-02-09 1:23 AM
There is no direct link between C and Assembly in this case. Inline assembly is handle ''like'' function, so there is no expectation that you will destroy registers and/or variables.
For more details, you can contact Cosmic support on their web page.