2006-02-17 1:38 AM
Configure a external EPROM ROM Memory on 0x0000h address
2011-05-17 3:10 AM
Hi, I want to configure de uPSD3333 using de PSDsoft Express to put a externar EPROM at the 0x0000h address.
The EPROM is conected using MCUADx PIN's, !PSEN and using a external LACH with ALE sinal. The object is to use the EPROM as a boot software. I need to boot on the external memory. The 0x0000h address is only boot address? Is posible to run software only on a External EPROM memory like we do on olds hardwars? Regards