Skip to main content
sagam
Associate
January 3, 2008
Question

Code and Data in the CSBOOT memory

  • January 3, 2008
  • 2 replies
  • 820 views
Posted on January 03, 2008 at 11:21

Code and Data in the CSBOOT memory

This topic has been closed for replies.

2 replies

jdaniel
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:51

sagam,

The flash memory banks in the uPSD are not write-while-execute capable. What this means is that if you're running code in CSBOOTX, you cannot at the same time program/erase ANY other CSBOOT area. You'll have to be running from RAM or from FSX (main flash) if you want to reprogram the CSBOOT sectors. This is the reason there are these two separate areas in the chip.

-Phaze426

sagam
sagamAuthor
Associate
May 17, 2011
Posted on May 17, 2011 at 11:51

I'm using the 3454 wit the main memory used as data and CSBOOT0-2 as code, and CSBOOT3 as programmable data page (in PSDExpress the sec. memory is defined as code&data - so the VM is good). Everything is working just fine but when I try to erase sector CSBOOT3 to write new data to it, the MCU will 'freeze' until reset. The CSBOOT3 is set to page 8 and mapped to 0x8000-0x9FFF as it should be. Writing to any sector of the main flash (using the same code different pages)works just fine. Can someone help and explain what I'm doing wrong, or point to a similar code example (code and data within the CSBOOT memory)? Thanks!