2007-08-25 3:17 AM
Clearing ENET Interrupts (ENET_ISR)
2011-05-17 12:46 AM
What is the proper way to clear the interrupt bits for the ENET_ISR?
Below is some code snippets. Is this the correct way to handle clearing the interrupt? Is there a better way? Is there something else I should do? I enable the following interrupts:ENET_DMA->IER = 0x00000000; // clear all bits
ENET_DMA->IER |= 0x02000000; // TX_MERR_INT_EN
ENET_DMA->IER |= 0x00800000; // TX_DONE_EN
ENET_DMA->IER |= 0x00400000; // TX_NEXT_EN
ENET_DMA->IER |= 0x00000200; // RX_MERR_INT_EN
ENET_DMA->IER |= 0x00000080; // RX_DONE_EN
ENET_DMA->IER |= 0x00000040; // RX_NEXT_EN
ENET_DMA->IER |= 0x00000020; // PACKET_LOST_EN
I enable the ENET interrupt vector
VIC_Config( ENET_ITLine, VIC_IRQ, 2 );
VIC_ITCmd( ENET_ITLine, ENABLE );
My ISR gets called okay:
void ENET_IRQHandler(void)
{
u32 currentState = ENET_DMA->ISR;
u32 irqToClear = 0;
if ( currentState & 0x00800000 ) // TX_DONE_EN
{
MUTEX_ENET = 1;
irqToClear |= 0x00800000;
}
// TODO: Check for Received packet
if ( currentState & 0x00000080 )
{
MUTEX_ENET_REC = 1;
irqToClear |= 0x00000080;
}
// TODO: Check for Errors?
if ( currentState & 0x00000020 )
{
irqToClear |= 0x00000020;
}
// Clear Interupt: Is this okay?
ENET_DMA->ISR = irqToClear; // 0xFFFFFFF
}
2011-05-17 12:46 AM
Hi
The method looks correct - simply write the bit to be cleared with 1. However I see no advantage in collecting the serviced interrupt bits and clearing them all at the end of the routine. Rather than doing irqToClear |= 0x00000020; you could simply do ENET_DMA->ISR = 0x00000020; Also it may be an idea to use a loop in the routine so that it only exits when all interrupt have been service (an interrupt can arrive while in the IRQ so it can be serviced without having to first quit. Eg: while ((ENET_ISR) & ENET_IER) { // while enabled interrupts waiting, handle them all if (ENET_ISR & TX_CURR_DONE_EN) { ENET_ISR = TX_CURR_DONE_EN; // reset flag // etc. } if (ENET_ISR & RX_ENTRY_EN) { ENET_ISR = RX_ENTRY_EN; // reset flag // etc. } // etc.... } Regards Mark