2006-06-19 7:14 PM
Change Baudrate of UART in Application
2006-06-15 5:26 AM
Dear RISC:
I develop an application. 9600 is the default of both Host and Client. Host sends command let Client changes to 115200. Client uses 9600 respone ACK to Host. Wait TXEmpty on , Client changes to 115200. Question: What is the flow which changes from 9600 to 115200 ? How many time is need to wait ? Because: I set a breakpoint at TXEmpty , Stop and Run. It is OK. If no breakpoint , Host needs to retry 2 or 3 times. Thank you.2006-06-19 7:14 PM
Thank you.
Because our project is so huge. We are follow the ModBus like Protocol. ex: We define : 0 : 9600(default) 1 : 19200 2 : 38400 3 : 57600 4 : 115200 function code : 0x32 PC -> :013204xx (9600) ST -> :013204xx (echo 9600 ok) I wait TXEmpty launched. Change Baudrate to 115200.(PC & ST) Both PC & ST delay 1 second PC -> :0103xxxx... (115200 request,it will timeout one or two times) After retry one or two times, ST responds correctly. I want to know what I need to do, when I pre-change or post-change baudrate ? Like Stop RX or....... Thank you.