2005-09-09 3:48 AM
2005-09-09 3:35 AM
Hello,
I have a PCB with 142 pin connected to a pull-up resistor. I use correctly a spi flash. After a minute, I enter in LPWFI mode and disable BPSI1 by a BSPI_Enable (BSPI1,DISABLE); command After an interrupt, the program restart and enable the bspi but the BPSI1 component detect a bus error. I don't understand why. Thank's,2005-09-09 3:48 AM
Sorry,
In fact the pin GPIO0.7 was used somewhere else. My mistake