2007-04-17 2:54 AM
2011-05-17 12:41 AM
Hi all,
When using the CAN_library, the APB_CLK is supposed to be 8MHz. I use 48MHz. Is it sufficient to multiply all the Bitrate prescaler values (BRP) in the CanTimings struct by 6? Microchip has a utility (Visual initializer)to calc the values that have to be entered into the registers to get the correct CANbitrate (In fact this utility can be used to initialize all the pheripherals on a PIC) . Does this exists for STR9 ? Kind regards, Luc.2011-05-17 12:41 AM
Thank you ...
Luc