2006-08-01 1:20 AM
2006-07-17 8:05 PM
Hi all, I m newbie in SPI. I am facing problem with the BSPI1 here. I have 2 board right now. One is ST710 and another is cypress board. I am using SPI to connect both board together. I set cypress board as Master, ST board as slave and connect the 4 pins together.
ST Cypress --- ------- MISO <==> MISO MOSI <==> MOSI SCK <==> SCK SS <==> SS I am testing to send 1 byte from Cypress(Master) to ST(Slave). i received correctly on the ST board. After that the problem occur when i want to send 1 byte from ST board(Slave) to Cypress board (Master). I am using the following method to send data over. Method ====== I noticed that Slave can't generate clock if they want to send data, the clock has to be come out from Master. So i connect another GPIO to interrupt the Cypress board, when i have something to send from ST (Slave) to Cypress(Master) i just pull high the GPIO to let the Cypress know something need to send over from ST. Before i pull high the GPIO line, i set my Data(1 byte) into the transmit register first in ST. After that i pull high the GPIO. Cypress will send a dummy data(generate clock) over in order to get the data from ST. So i get the data now in Cypress Receive register. Problem ======= Let say, I want to send 0xA0 from Cypress to ST. ST send 0x12 to Cypress. 0xA0 1. Cypress ======> ST. 0x12 2. ST ======> Cypress. The sequence is i send 0xA0 first from Cypress to ST. I receive correctly. Then in ST i set 0x12 into transmit register. After that i pull high the GPIO line. Cypress will send dummy data over. The problem is the data shifted out is not the 0x12, but it is the data i send from Cypress 0xA0. I use oscilloscope to see, it is 0xA0. My 0x12 only get send on the next byte. I check the status register before i want to write into the transmit register in ST and it is not FULL(TFF), i set the FIFO depth to 1 byte. I am suspecting the Shift register is not clear yet, it still contain 0xA0. Any help or suggestion ? SPI configuration (ST BSPI1) ================= GPIO_Config (GPIO0, 0x00F0, GPIO_AF_PP); BSPI_Init ( BSPI1 ) ; BSPI_ClockDividerConfig ( BSPI1,96); // 24 MHz / 96 = 250KHz BSPI_Enable ( BSPI1 , ENABLE ); BSPI_MasterEnable ( BSPI1,DISABLE); BSPI_ClkActiveHigh(BSPI1,ENABLE); BSPI_ClkFEdge(BSPI1, ENABLE); /* Set the word length to 8 bit */ BSPI_8bLEn(BSPI1,ENABLE); BSPI_TrFifoDepth(BSPI1, 0); BSPI_RcFifoDepth(BSPI1,0); BSPI_RcItSrc(BSPI1, BSPI_RC_FF); [ This message was edited by: JJz on 18-07-2006 14:06 ]2006-07-19 12:54 AM
i have tried this setting, my problem still not solved. Any other idea ? Why the value is still keep in the shift register after i have read the receive fifo? thanx.