cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-LP: Recently (Feb 2022), you have released the Evaluation Tool STEVAL-IDB011V2. The BLE-RF-output has been CHANGED compared to STEVAL-IDB011V1 (now NRND)

WLech.1
Associate II

Is the modified RF-output filtering better in terms of EMI for FCC or CE-certification?

The new filtering in V2 consists of two filtering stages and replaces one integrated filter 2400-2500 MHz.

What is the reason for this change and why did you set STEVAL-IDB011V1 to "not recommended for new design"?

STEVAL-IDB011V1:

0693W00000KbgCXQAZ.png STEVAL-IDB011V2:

0693W00000KbgDzQAJ.png 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @WLech.1​, to the community!

the performance is the same.

As indicated in UM2735, section 2.1, STEVAL-IDB011V2 differs from its predecessor STEVAL-IDB011V1 in only two details:

  • U2 (integrated filter in V1) replacement with discrete components (in V2) and
  • CN7 replacement with a 1x4 footprint

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @WLech.1​, to the community!

the performance is the same.

As indicated in UM2735, section 2.1, STEVAL-IDB011V2 differs from its predecessor STEVAL-IDB011V1 in only two details:

  • U2 (integrated filter in V1) replacement with discrete components (in V2) and
  • CN7 replacement with a 1x4 footprint

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
WLech.1
Associate II

Hi Peter,

Yes - thank you for your quick response.

I take both filtering solutions as equal!

best regards,

Walter

OK, good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.