2011-02-02 9:19 AM
We are proud to annunce the release of
v0.8eLua is an effort to expand the presence of the Lua programming language in the embedded world, especially on microcontroller-based platforms. It is meant to be a complete MCU development environment. It currently runs on a number of ARM variants (including Cortex-M3), AVR32 (and i386 as a proof of concept).
The main changes from v0.7 are:
* Added the RFS (Remote File System), a new file system which allows sharinga directory on the PC with the eLua board.* Added a serial multiplexer which allows using more virtual serial ports over a single physical UART connection.* Added Lua and C interrupt handlers support.* Added linenoise support (eLua and Lua shell command line history and navigation)* Added generic I2C support and docs* Added hardware flow control and runtime configurable buffers for UARTs.* Added support for new boards: mbed, EVK-1101, Mizar32, EK-LM3S1968* Added SPI and SD/MMC support for EVK1100 and EVK1101 (AVR32) * Added I2C support for STR-E912 (STR912) * Added support for require() and autorun from SD/MMC* Added external memory support for STR912* Added long filename support for SD/MMC* Added version() function to elua module* Added RTC (real time clock) platform specific support for str9* Added support for AsciiDoc in the doc builder* Tutorials and new projects added to the eLua User Labs wiki* Demo files were moved out of the distro tohttp://wiki.eluaproject.net/Projects
* eLua wiki: * Mail list:https://lists.berlios.de/mailman/listinfo/elua-dev
http://builder.eluaproject.net/
* Issue tracker: * Other: