cancel
Showing results for 
Search instead for 
Did you mean: 

adc resolution

swiggers9
Associate II
Posted on September 21, 2006 at 06:03

adc resolution

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
hichem2
Associate II
Posted on September 21, 2006 at 05:55

Hello,

In the ADC spec there is the following note:

Any added external serial resistor will downgrade the ADC accuracy (especially for resistance greater than

10kΩ). Data based on characterization results, not tested in production.

Regards,

Hich

swiggers9
Associate II
Posted on September 21, 2006 at 06:03

ok, but if you mean the circuit with the potentiometer, I'm not using that one. I have a filtered voltage regulator as adc source.

In the schematic you can also see that AVss is connected to DGnd. is this ok? or should AGnd and DGnd be separated?