2006-09-20 9:03 PM
2006-09-20 8:55 PM
Hello,
In the ADC spec there is the following note: Any added external serial resistor will downgrade the ADC accuracy (especially for resistance greater than 10kΩ). Data based on characterization results, not tested in production. Regards, Hich2006-09-20 9:03 PM
ok, but if you mean the circuit with the potentiometer, I'm not using that one. I have a filtered voltage regulator as adc source.
In the schematic you can also see that AVss is connected to DGnd. is this ok? or should AGnd and DGnd be separated?