cancel
Showing results for 
Search instead for 
Did you mean: 

About the use of the M24C64-FMC6TG with the I3C bus

Clavin-z
Associate

"Does the M24C64-FMC6TG have a spike filter that allows it to be mounted on an I3C bus and operate at maximum speed?"

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Clavin-z, to the community!

The M24C64-FMC6TG came onto the market long before 2010, whereas I3C was not developed until 2016. In this respect, the topic of spike filters was still unknown at the time the M24C64-FMC6TG was launched and is therefore not yet included.

Does it answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.