2006-01-12 3:27 AM
2006-01-11 7:47 PM
Hi all,
Does someone know if it is possible to connect 3 SPI devices on one SPI bus? I have 2 touchscreen controller/driver IC's both with a SPI bus output and I want to connect them to the same SPI bus on my STR710 microcontroller.(I can not use the second SPI of the STR710) Is this possible? Thanks, Jimmey2006-01-12 3:27 AM
Yes you can.
You just need to make sure you only select one device at a time (i.e. control the chip select inputs on the slave devices...in your case it will be your touch screen controllers). Best regards, Ryan.