2017-11-01 01:29 AM
How do I change the regulation mode from Secondary to Primary in eDesignSuite?
I want to design a low cost 85-265V AC to 12V 0.2A DC isolated flyback converter using the Viper06 with PSR.
Tight Voltage Regulation and Fast Transient Response is not required, so we want to save cost of optocoupler.
Kind Regards
#viper #viper06 #psr-cv2017-11-02 03:53 AM
Hello,
First of all you need to change the schematic, following the sample circuit in VIPer06 datasheet, figure 20.
Then the compensation net and the transformer, too, must be designed in a slightly different way, we are working to add this feature in eDesign as soon as possible.
Best regards.