2008-08-21 12:16 AM
with and without marking A of uPSD3454EB40T6 ? USB affected!
2011-05-17 02:52 AM
according to the PCN attached, the marking A only related to bond pad re-layout,which should not affect the functionality,
1, however, the USB does perform OK with marking A, but failed in PC cold boot without marking A! Is the USB function really the same between these 2 chips! 2, the marking A should be newer since it is new revision, but the attached photos show the one without marking A is newer! Why?