cancel
Showing results for 
Search instead for 
Did you mean: 

Vl53l5CX coverglass

smenet
Associate

Hello,

i am currently testing the vl53l5cx lidar sensor without a coverglass, but i will need soon to use a coverglass(dusty environment). When using the coverglass, can the vl53l5cx (with Xtalk calibration) still detect object at close range(from 2cm to 60cm)? And when using the coverglass, do the vl53l5cx still need a calibration with Xtalk for far away object(>60cm)?

Thank you

0 REPLIES 0