2007-11-21 04:57 AM
2011-05-17 12:41 AM
Hi MBS
When I try to complie the project in Anglia IDE I receive the following warrings: In file included from ./../../library/inc/91x_vic.h:27, from ../../library/src/91x_vic.c:21: ./../../library/inc/91x_it.h:44: warning: empty declaration ./../../library/inc/91x_it.h:45: warning: empty declaration ./../../library/inc/91x_it.h:66: warning: empty declaration What's going wrong? Regards. Greg And when I try to compile project in Release Mode I receive errors: E:\Technika\Szkolenie_ARM\ARM_forum\IRQ_anglia_IDE\str91xstdlib\Stdlib\project\91x_it.c -march=armv5te -mapcs -g -Wall -O0 -Iuip -Ienet ../91x_it.c:51: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'void' ../91x_it.c:153: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'void' ../91x_it.c:372: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'void' ** Errors Detected in Build ** Greg [ This message was edited by: GrzesiekFl on 13-04-2007 18:32 ]2011-05-17 12:41 AM
Hi GrzesiekFl,
Quote:
When I try to complie the project in Anglia IDE I receive the following warrings: ./../../library/inc/91x_it.h:44: warning: empty declaration ./../../library/inc/91x_it.h:45: warning: empty declaration ./../../library/inc/91x_it.h:66: warning: empty declaration it was due to this:Quote:
#ifdef __GNUC__ /* GCC Compiler */ #define interrupt __attribute__ ((interrupt)); #define irq interrupt #endif in fact,with an interrupt function the declaration should be as follow :Quote:
void FOOxxxx (void) __attribute__ ((interrupt)); :-o the problem now is : why it works fine with RIDE compiler (which uses GCC-ARM) and doesn't with ANGLIA ? 8-) I'm investigating ... in meanwhile, please find attached the corrected project. Best regards, MBS[ This message was edited by: MBS on 16-04-2007 11:44 ]2011-05-17 12:41 AM
Hi MBS
Sorry, but this program doesn't work. It compiles correct, but the interrupts stop program If I switch off interrupts //VIC_ITCmd(TIM0_ITLine, ENABLE); //VIC_ITCmd(RTC_ITLine, ENABLE); program works correctly I think the problem is in section #define IENABLE asm('' MRS LR, SPSR''); /* Copy SPSR_irq to LR */ asm(''STMFD SP!, {LR} ''); /* Save SPSR_irq */ asm(''MSR CPSR_c, #0x1F ''); /* Enable IRQ (Sys Mode) */ asm(''STMFD SP!, {LR} '') ; /* Save LR */ #define IDISABLE asm(''LDMFD SP!, {LR}'') ; /* Restore LR */ asm(''MSR CPSR_c, #0x92'') ; /* Disable IRQ (IRQ Mode) */ asm(''LDMFD SP!, {LR}'') ; /* Restore SPSR_irq to LR */ asm(''MSR SPSR_cxsf, LR'') ; /* Copy LR to SPSR_irq */ I just added delay() function and port GPIO7 (diodes), I use MCB-STR9 starter kit Regards, Greg2011-05-17 12:41 AM
hi GrzesiekFl,
Sorry, i've tried this example with IAR and RIDE and it works fine but i've just compile with ANGLIA .(no flash link)Quote:
I think the problem is in section #define IENABLE asm('' MRS LR, SPSR''); /* Copy SPSR_irq to LR */ asm(''STMFD SP!, {LR} ''); /* Save SPSR_irq */ asm(''MSR CPSR_c, #0x1F ''); /* Enable IRQ (Sys Mode) */ asm(''STMFD SP!, {LR} '') ; /* Save LR */ #define IDISABLE asm(''LDMFD SP!, {LR}'') ; /* Restore LR */ asm(''MSR CPSR_c, #0x92'') ; /* Disable IRQ (IRQ Mode) */ asm(''LDMFD SP!, {LR}'') ; /* Restore SPSR_irq to LR */ asm(''MSR SPSR_cxsf, LR'') ; /* Copy LR to SPSR_irq */ try the attached project, i've just deleted these functions and replace them by their code in the different interrupt functions. 8-) Best regards MBS2011-05-17 12:41 AM
Can somebody explain IDISABLE and IENABLE macros. In my project when I leave interrupt with IDISABLE macro at the end my program stops.
I still have problem with this VIC0 and VIC1 problem, can somebody overcome this problem finally. I need a sample code for Anglia Compiler with two interrupts with form different VIC's, Please help because my boss will kill me :-) best regards, J.O.