2005-03-04 01:50 AM
2005-03-03 05:28 AM
2005-03-04 01:50 AM
Hello Avnet_FAE,
Bellow you find some HDLC Caracteristic used to determine maximum speed using HDLC and Manchaster coding, The STR71x HDLC has been used by customer in the following conditions: TX: 921KBit (manchester) RX: 250KBit (NRZI) Anyway our engineer verified that the maximum baudrate could be: TX: APB clk (APB=32MHz), but, due to the fact that the pad cannot reach more than 16MHz, clock in TX should be divided, at least, by 2. RX: APB clk/16. hope this can help you. With regards, Hich :-?