cancel
Showing results for 
Search instead for 
Did you mean: 

Use of EV-L99LDLH32GEN development board

Jing_H
Associate

1. Regarding the development board: Does EV-L99LDLH32GEN require an external driver to work? Or does the development board come with its own driver chip?

2. In addition to driving LEDs, can it also drive other loads?

 

This post has been translated from Chinese to comply with the ST Community guidelines.

 

 

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Jing_H, to the community!

  1. the board EV-L99LDLH32GEN contains two 32-channel LED / OLED driver with automotive CAN FD Light interface chips L99LDLH32, with which O/LED can be controlled directly.
  2. you can certainly also drive other loads if they fit the specifications of the L99LDLH32 (e.g. 32 channels, constant current, high side driven, 1...15mA/channel). What other loads do you want to drive?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.