2004-07-15 04:58 AM
2004-02-26 08:52 PM
How to disable the USB of STPC Atlas ? Does whcih register can do it ?
Can't find any information for this.2004-03-02 04:15 AM
2004-07-15 04:58 AM
I face the same issue.
With the programing manual version 1.0, this register has a different definition. It looks like these bits are now read-write thus the accesses can be disabled and the various OS detection routines could not see it. I will need to free IRQ lines for a legacy design, so I have to disable the interupt lines associated to the USB also. Has anyone done this? Felix