2024-10-21 09:08 AM
Good morning,
In a university project we are using an nRF24L01 chip to produce a signal, which is then split and modulated by means of other devices.
The final stage of each of the split signals is a AD8341 chips which has a 50ohms differential output.
This chip then feeds a ducky antenna via an SMA connector, and as per Analog Devices application notes, a balun is recommended.
I was wondering if there's any hint about the performances of the BAL-NRF01D3, if placed at the output of the AD8341. Or, if there's any hint about being it strongly discouraged.
Additionally, is there any data available about the phase unbalance of the BAL-NRF01D3?
I remain available for clarification, thank you in advance and
Best regards
Francesco