2011-08-09 02:23 PM
Is it possible to use the STVP in a Windows XP environment with either a USB or PCI-e based ExpressCard Parallel Port adapter? So far, I'm not having any luck as the software refuses to install the ParSTm driver because the parport service is not running. The parport service won't start because it complains that it cannot find a device to use it with despite having correctly installed both of the previously mentioned adapters.
#driver #parallel-port #stvp