2007-07-19 10:44 PM
STR9 V1.2 library New Release and MCU for optimum CPU performance
2011-05-17 12:44 AM
Hi Eris
I have found that I have no problem with STR911-REV.G at 96MHz but my STR912-REV.F does. However I may receive an STR912-REV.G soon. Since I have also older STR912 I am using the Ethernet projects at 48MHz zu avoid any issues. For the moment I am not doing any more tests here but there are a few Beta testers of our OS and TCP/IP stack which will hopefully give feedback to identify whether it is a chip or project problem. They tend to have older chips on teh demo boards (of course) Regards Mark