cancel
Showing results for 
Search instead for 
Did you mean: 

STR9 V1.2 library New Release and MCU for optimum CPU performance

amira1
Associate II
Posted on July 20, 2007 at 07:44

STR9 V1.2 library New Release and MCU for optimum CPU performance

10 REPLIES 10
m_j_butcher
Associate II
Posted on May 17, 2011 at 09:44

Hi Eris

I have found that I have no problem with STR911-REV.G at 96MHz but my STR912-REV.F does.

However I may receive an STR912-REV.G soon.

Since I have also older STR912 I am using the Ethernet projects at 48MHz zu avoid any issues.

For the moment I am not doing any more tests here but there are a few Beta testers of our OS and TCP/IP stack which will hopefully give feedback to identify whether it is a chip or project problem. They tend to have older chips on teh demo boards (of course)

Regards

Mark